Part Number: LMH6703
Tool/software:
I have an LMH6703 working from +9V and neg3V split supplies. in the data sheet there is a phrase about "For 5-V supplies only, the LMH6703 has a TTL logic compatible disable function"
does that mean the disable function cannot operate in my configuration? or it just means that different voltage levels are required to disable?
there is also reference to low being <0.8V, and also "to prevent the shutdown pin voltage from going more than 0.8 V below the midpoint of the supply voltages.
SO I understand in my case- where midpoint is +3V, I would need a voltage between 2.2V and 3.8V to disable?
and a voltage above +5V as a logic high - to what maximum? and would 4.9V work?
ALSO - WHEN DISABLED - WILL THE OUTPUT GO LOW RAIL? TO MIDPOINT? OR?
also - I see a typ 10ns time for enable and disable - is there a maximum time?
thanks
Pinhas