This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXU0104:Question about maximum ratings

Part Number: TXU0104

Tool/software:

Hello,

I am using a TXU0104PWR. I am using it to convert the level of a BUS communication line, and when I checked the waveform, I found that some parts were below -0.5V due to noise.

This is outside the range of 7.1 Absolute Maximum Ratings in the datasheet, but

it states "(2) The input voltage and output negative-voltage ratings may be exceeded if the input and output current ratings are observed."

The current does not reach -20mA, so it is within the range, so is it okay to use it this way?

Regards