Tool/software:
The datasheet mentioned default short-circuit current when Vcl is left floating but not output current.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The datasheet mentioned default short-circuit current when Vcl is left floating but not output current.
Hello Shubhangi,
To clarify, are you wondering what the output current is when Vcl is left floating?
For your second question, are you using single supply configuration?
Thank you,
Sima
Hello Shubhangi,
If Vcl is floating, the output current will be the maximum of the device: 700mA. At elevated temperatures this current will decrease. It is not recommended to operate the device at its maximum continuously and it is highly recommended to drive the pin.
For dual supply configuration: you may ground the GND pin and drive the CL pin (VCL or VPROG) with the correct voltage based on Rext. You must be careful in choosing Rext, as you should not violate the maximum CL to GND voltage of +/- 1.2V.
Iext = Vprog/Rext (current into pin)
Through the VCL pin, IOUT is programmable from 10 mA to 300 mA by setting Iext (current into VCL pin) from 25 μA to 750 µA by means of a fixed Rext of 10 kΩ and making Vprog variable from 0.25 V to 7.5 V.
Therefore two items to watch out for when setting this pin:
Both can be controlled by tunning Rext value.
Thank you,
Sima
Hi Sima,
is 700mA short circuit current or continuous output current? Wouldn't the output current depend on kind of load connected?
My another question still remains- if I use Vprog=+2.5V and Rext=10k, will it work? what will be value of Vcl in this case?
Thanks,
Shubhangi
Hello Shubhangi,

The noninverting pin is connected to ground at the internal amplifier, therefore inverting pin is equal to 0V at that node.
Thank you,
Sima