Part Number: OPA355
Tool/software:
Hi there, The power supply setting for OPA355 is ±1.8V. What should be the logic level for controlling the enable pin,
I see that the low level is less than 0.8V, and the high level should be greater than 2V. When using a split-supply, the enable and disable voltage levels are referenced to V–.
So, does this mean the low level should be less than -1V and the high level should be greater than 0.2V?
How should I set it? For example, can I use 3.3V for the high level and 0V for the low level? Thanks