This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903-Q1: Changes Revsion L → M

Part Number: LM2903-Q1
Other Parts Discussed in Thread: LM339

Tool/software:

Hi all,

I have some questions about the graph Updated Typical Characteristics below.

1) I understand that each graph has different measurement conditions. Please tell me each measurement condition.

Revision L→Figure 1

Revision M→Figure 2-1TA = 25°C, VS = 5V, RPULLUP = 5.1k, CL = 15pF, VCM = 0V, VUNDERDRIVE = 100mV, VOVERDRIVE = 100mV unless otherwise

L:M

2) I think there is a difference in the block diagram.

Q9~12, Q14 and Q15 have been added.

This circuit was changed due to the addition of the previous process plant.

Is that correct? Or was it there originally?

Best Regards,

Ryusuke