This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2376: if TI have the same pakage as ISL24021

Part Number: OPA2376

Tool/software:

Hi sir

due to the parts EOL

May i know if TI have the same pakage as ISL24021 

  • Chen,

    The ISL24021 is a high output current, high voltage (max supply 19V), rail-to-rail voltage feedback amplifier capable of ±1A peak output short circuit current and to drive large continuous currents of ±300mA.  OPA2376, on the other hand, is a low supply voltage (max 5.5V) with max output current of +/-30mA (max 10mA at 125C) so it's a complete mismatch between the two.   But to answer your question, we do not offer op amps in 8 LD TDFN package.