Part Number: OPA2891
Other Parts Discussed in Thread: OPA567
Tool/software:
Hello dear members of the team,
i need to design a supercapacitor balancing circuit, i have 8 supercaps in series and i would like to balance it with operational amplifiers.
I attach a design with opa2891 used to balance the caps, but this circuit is totally not working. I understand that this opa2891 needs 9V between supply pins to operate, so, in this design, it will not work until the voltage at the cap series is above 9V. But it isn't working anyway, even with series' voltage > 9V.
- I can't understand why. Do you have any suggestion? Is there a correction that should i do?
- Can the OPA567 be a better option than OPA2891?
Thanks if you have any hint,
Kind Regards
emazed