Part Number: TLV7031
Other Parts Discussed in Thread: TLV1831
Tool/software:
Dear Team ,
My circuit and it's output wave-from is given below.

The green color is the output waveform. The amplitude varies from 0 to 2.1V.
This output will be given to a comparator and at the comparator output also I need the same green signal.
Actully for making it clean we are proving it to a comparator.
Below is the initial comparator circuit.

The comparator output currently I am getting is zero.Below is my board file

I tried to simulate the comparator using Tina TI.The circuit shown in the board is given below.
It is working in simulation but not in board.May I know where I went wrong.In the simulation you can see comparator output ramping from zero.
The signal data rate is UART 9600

Do I need to move to open loop.
Regards
HARI