This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA241B: INA241 NC Pin

Part Number: INA241B

Tool/software:

Hello,

I'm working on a servo driver board with inline current sensing. Initially, I used AD818 current sense amps but after testing decided to switch to INA241B2. The chips appear to be pin for pin compatible, except the NC pin. INA241 datasheet says to connect it to GND, AD8418 datasheet says to leave that pin floating. Since the boards were originally designed for AD8418, the prototype boards have that pin floating.

I soldered INA241B2 in place without connecting the NC pin to GND and everything seemed to work fine. It's working a lot better than AD8418, so I'm planning to use INA241B2 for production (might also test INA241A2 before to see if it's worth the price difference). For the production boards, I can edit the design to connect the NC pin to GND before ordering the boards. My question is, is the pin connected internally to the chip? Does it matter if I leave it floating or should it be connected?

  • Hello Isik,

    My question is, is the pin connected internally to the chip?

    Yes it is connected internally to the device.

    Does it matter if I leave it floating or should it be connected?

    It normally does not matter but floating pins can sometimes cause issues as they can interact with other unexpected things.  I would highly recommend you connect pins as recommended in datasheets.  In this case I would recommend you connect to GND. 

    Regards,

    Javier