Part Number: TLV1852
Other Parts Discussed in Thread: TLV1862, TLV1812, LMC6762
Tool/software:
Good morning,
I need to know what the differential input resistance and common mode resistance of the TLV1852 comparator are.
Bye
Banchini Tommaso
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Banchini.
There is IIB spec. Current at just one input point.

There is this chart. High current for input greater than supply voltage

Zoom in, roughly 1nA at 0V and 125C; So 1.8V and 1nA = 1.8 G ohms

Current does not flow input to input, so differential input resistance is very high.
I tried but it does not meet my requirements. I have a source with an impedance of 1MOhm, and I therefore need a comparator that has a minimum differential input resistance of 1GOhm. Using the TLV1862, I still have a considerable (measured) loss. What can I do? Premise: I cannot use buffers between the source and the comparator, I need a clean and direct connection.
I tried but it does not meet my requirements. I have a source with an impedance of 1MOhm, and I therefore need a comparator that has a minimum differential input resistance of 1GOhm. Using the TLV1862, I still have a considerable (measured) loss. What can I do? Premise: I cannot use buffers between the source and the comparator, I need a clean and direct connection.
I tried but it does not meet my requirements. I have a source with an impedance of 1MOhm, and I therefore need a comparator that has a minimum differential input resistance of 1GOhm. Using the TLV1862, I still have a considerable (measured) loss. What can I do? Premise: I cannot use buffers between the source and the comparator, I need a direct connection
Tommaso,
What is your supply voltage, input voltage range and speed requirement?
I can find a higher impedance input, one that doesn't use input as a supply source.
Ron
I have a power supply of +5V and -5V; I would possibly need a rail-to-rail input amplifier with no speed requirements (we're talking about a response time on the order of 100us).
LMC6762 has the lowest input current so the highest input impedance. TLV1812 is also good if temperature range is not too big.
rail-to-rail input amplifier
Is the original request for comparator still correct?