Part Number: OPA855DSGEVM
Other Parts Discussed in Thread: OPA858, OPA855
Tool/software:
I am using the OPA855 in a TIA circuit. The input is a capacitive sensor with a capacitance of approximately 50pf with resulting currents estimated around 50pAmps. The issue I have is that an offset exists on the V- of -200mV measured at (In). I also have the circuit constructed just as shown with no sensor connected between the (In) and GND, and I get the same -200mV offset. I have ordered the OPA858 to see if that works better.
Supply voltages are +2.5V and -2.5V.
Any thoughts on this?
Schematic of what I am doing is shown.

Thank You,
Phillip Snyder