This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5157: LM5157 for 27V Fixed Output from 18–36V Input (750 mA to 1A Output Current)

Part Number: LM5157
Other Parts Discussed in Thread: LM5177

Tool/software:

Hi TI Team,

I’m planning to design a power supply that provides a fixed 27 V output at up to 750 mA (ideally 1 A if possible), from a variable input voltage range of 18 V to 36 V.

Could you please confirm if the LM5157 is suitable for this application? If so, I would appreciate it if you could share a recommended reference design or schematic for this configuration.

If the LM5157 can support up to 1 A output current at 27 V, that would be even better.

Also, if you have any other suitable solutions or alternative configurations for this requirement, please let me know.

Thanks in advance for your support!

Best regards,

Manikandan V