This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9002: Schematic Review for insulation monitor

Part Number: TLV9002


Tool/software:

Hi,

Can you please help review the sensing circuit for TLV9002 on pg 2 of the schematic?  This is for an insulation monitor ref design.

The HV input range is -1kV to 0V for the negative side, 0V to 1kV for the positive side, and ADC VREF is 3.3V.

thanks

-kelvin

8715.TIDA-010985E1(001)_Sch.PDF