Part Number: LMP8481
Tool/software:
Hello TI team,
I am currently working on Battery Management System(BMS) project and using the LMP8481MM high-side current sense amplifier(Bi-directional) for current measurement. However, i am facing repeated current sensing failures during operation.
I would appreciate guidance on the following:
1.What are the common failure modes of the LMP8481 in such applications?
2.Are there recommended protections or design considerations for high-side sensing in BMS?
3.Is there any known issues with input differential voltage limits or transient spikes that could damage the part?
4.How can i debug whether the issue is due to the amplifier, shunt resistor(0.0003ohm) ?
Thanks in advance for your support!.