This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMV358-N-Q1: LMV358Q1MAX/NOPB Maximum input voltage

Part Number: LMV358-N-Q1


Tool/software:

Hello,

We are supplying V+ of LMV358Q1MAX/NOPB with 3.3V which is rated for maximum 5.5V and maximum input voltage is same as supply voltage.

Can we supply VIN+ or VIN- with 5V even though V+ is 3.3V? Could you please confirm!

  • Hello Asha,

    No because that would exceed the AMR table below.

    Also the LMV358-N-Q1 input common mode range is not rail to rail input.

     

    For what reason is the input voltage greater than supply? Would reducing volage with a resistor divider be a solution?