Part Number: INA138
Tool/software:

How would I extend this design to work with sources as high as 700VDC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA138
Tool/software:

How would I extend this design to work with sources as high as 700VDC
Hello Bruce,
This circuit design: https://www.ti.com/lit/an/sboa295a/sboa295a.pdf goes through the design process. I think the limiting factor for the voltage will be dominated by Q2 in image above which is Q1 in the design I have shared the link for.
The schematic that you attached also has a guide https://www.ti.com/lit/ug/tidu833/tidu833.pdf that mentions this as well in section 3.3 PNP Transistor
Regards,
Javier
Bruce,
Basically the supply voltage is provided with the Zener voltage. The two components are Q1 and R3 in the image below that must tolerate your high to low voltage transition. I assume either a higher voltage transistor or stacked transistors could work but please keep in mind what current you lose through leakage and power on the R3 with maintaining a current across the zener to keep it active during your circuits full operation condition. I would suggest simulation to confirm. You can start with this: https://www.ti.com/tool/download/SGLC001

I understand the requirement for sufficient current through the zener.
I attempted TINA simulation but could not find the way to add the INA138 to the schematic
Bruce,
Did the link above I sent you not work. It has the INA138 in that tina simulation file. You could simply cut an paste into your existing design.
Regards,
Javier
Got the link, thank you.
Next question is , could this be modified to use a MOSFET instead of the PNP bipolar transistor?
Hello Bruce,
Yes it can. See section 3.3 https://www.ti.com/lit/ug/tidu833/tidu833.pdf. Below for convenience.

Regards,
Javier
I am not finding PMOS that will work properly.
Back to the PNP bipolar
Trying to stack 2 devices to get higher voltage breakdown
not getting proper biasing configuration
Bruce,
You just have a voltage divider and the current goes through the resistor rather than the transistors. Also please be aware of the power on the resistors.

One more thing.
If I want to protect the INA138 against large current overloads (such as a short circuited load) , can I use a series resistor and clamp diode across the input terminals?
Hello Bruce,
This can be done and we have some documentation (https://www.ti.com/lit/ug/tidu473/tidu473.pdf) on this but you need to be aware that the INA138 is floating relative to your main ground so placing the protection needs to be to GND of the device. All absolute max ratings need to be avoided and they are relative to the GND of the device. Keep in mind that resistance into the device will also cause some gain error. Some of our other devices we recommend under 10Ω in series because of this.
Most of our devices are more concerned of the voltage changes during a transient current or short circuit event rather than the current itself so keep that in mind as you design your protection for the INA138.
If you explain the potential event that you are protecting from I can see how that would impact the INA138. I do normally a transient simulation with the conditions and add parasitics expected in the system to get a rough idea of voltages and currents. I have seen this as a good tool to find what I will need to protect from and the speeds required.
Regards,
Javier
Hello Bruce,
This will be an issue as you are creating a resistive path from the Rshunt to VIN- creating a voltage drop. These devices are not exactly like amplifiers and have an IB in the µA range. This will cause
Also from your schematic are you assuming R1 is damaged and open? Would the R1 accept power of 4watts. 2V*2V*/1Ω? I say 2V as that is our Absolute Maximum Voltage rating differentially at our inputs. Most of the current will flow across R1 and I think that will get damaged first before the INA138.
Regards,
Javier
I intend to limit the current flow with a fast acting fuse in the source.
The sense resistor would only see a momentary high current (.25 W rated resistor)
My only concern is exceeding the maximum differential voltage on the INA138
Please advise