Part Number: TL074
Tool/software:
Hi team,
My cutsomer wants to generate a 1.5V voltage reference for 1.5V offset input of 10x amplifiers.
They want to add iso resistor behind the amplifier's output. As you can see, there are three caps on the output. On the other 10x amplifiers' side, each input end of amplifier, there will be a 100pF.

10x amplifiers:

Q1: What is the suitable R193 value for this case? can you show the calculation formula.
We find a circuit stability analysis document.


It uses zero point frequency to get the resistor.
Q2: how to get above waveform then to get the zero point.