This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA857EVM-978: Using the board at 250V for APD Bias

Part Number: OPA857EVM-978


Tool/software:

Hello,

I want to use this board with an APD that needs 250V DC for bias. If I remove C4 and C5 capacitors, I think I can apply 250V DC bias. Please let me know.

Best Regards,

Amar Gaikwad

  • Hello Amar,

      You do not need to remove C4 and C5 capacitors to apply 250V DC bias. These capacitors are on supplies is used to suppress high-frequency noise in power supply signals. It also helps provides high transient currents to an IC if needed in high output current design.  You may be confusing these capacitors as AC coupling capacitors that block DC signals/information from an input/output. These capacitors are in series to input/output source to load, compared to decoupling capacitors that are placed in parallel to these DC supply sources. 

      Therefore, you may apply the 250V DC bias to VAPD (TP3).

    Thank you,

    Sima