Part Number: AMC1351
Other Parts Discussed in Thread: TLV6001, , INA597
Tool/software:
Hello, this is Ken.
I have a question about the circuit in Figure 8-3, listed in section 2.2.2.2 Differential to Single-Ended Output Conversion in the AMC1351 datasheet. I want the voltage applied to the AMC1351's IN to be the same as the voltage output from the TLV6001's OUT (in other words, I want to set the total gain to 1). What are the optimal values for R1, R2, R3, R4, C1, and C2 in this case?
Also, please tell me the formula for calculating the TLV6001's OUT value from the AMC1351's IN value.
The input voltage specifications for the circuit are as follows:
The AMC1351's VDD1 and VDD2 and the TLV6001's V+ are 3.3V, VREF is 1.65V, and the AMC1351's input voltage range is 1.65V to 2.75V.
Thank you in advance.