Other Parts Discussed in Thread: INA333, OPA2333, OPA2188, TINA-TI
Hi,
I'm designing an EMG measurement device to control a robotic hand, for a research project. The instrumentation amplifier I'm using as a preamplifier is the INA333, since is a widely used biopotential amplifier due to its characteristics. I'm having some trouble with it, the output signal is not as it sould be. I've done some tests with OrCAD Pspice, using sinewave signals as the inputs. Also I've done tests with the real circuit assembled in a breadboard, using sinewave signals too. The results are the same, the amplifier only outputs the positive (or negative if the difference is negative) half of the signal. This happens when I use a single power supply and a reference voltage with a value of half the power supply. When I use a dual power supply and a reference of 0V, everything works as expected and I am even able to measure the EMG signal.
I don't know what is the problem. The schematic is based on the ECG one that is in the datasheet of the INA333, and I think it's OK. I've attached the circuit schematic and the output signal generated by Pspice, in case you find any mistake that I've missed.
Thank you in advance, and excuse me for any mistakes in the text as English in not my native language.