Part Number: AMC1311
Other Parts Discussed in Thread: TINA-TI
Tool/software:
Hi,
I am using AMC1311 for voltage sending in my Dual Active Bridge. Schematics is given below. I am using an isolated 5V to power the left side Vdd1 another isolated 3.3V to power the Vdd2. And the AMC1311 is also isolated. Do I need a level shifter at the output of the sensor that is going to my differential amplifier then to my 3.3V ADC in my MUC?
Or since I am using an isolated 3.3V to power the isolated AMC1311 sensor, level shifting is not necessary here ?