Part Number: INA333
Tool/software:

The circuit above shows a 3-wire RTD PT100 reader. I've measured the output current from pins A1-B2 and B1-B2 at 1mA each. VDD = 5V, GNDA = 0V.
I'm using a resistance generator to simulate an RTD. When the resistance is 100 ohms, the voltage measured between the Vin+ and Vin- pins is 0.098V, while the INA333 output pin measures 0.49V.
When I increase the resistance, for example, 200 ohms, the voltage measured between the Vin+ and Vin- pins is 0.197V, but the INA333 output pin measures 0.658V. Is there something wrong with my circuit?