This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR111-2EVM: It is still not working

Part Number: XTR111-2EVM
Other Parts Discussed in Thread: XTR111

Tool/software:

AC220V outputs AC24V through a power frequency transformer and converts it to DC24V through a rectifier bridge, isolating the DCDC and outputting CPU voltage. The CPU outputs dac0-3.30v 50hz communication encoding waveform, inputs xtr111, and xtr111 outputs 0-20mA, which is connected to ac24 positive through cbb capacitor, and then returns ac220v through power frequency transformer to report communication encoding information. The AC24 load is 600mA. In communication, this principle of connection feels no change. Has it been submerged. The solution chip is still not working.