Part Number: LMH6552
Other Parts Discussed in Thread: LMH5401, , DAC37J84, THS4567, OPA858, OPA855
Tool/software:
Can I use the LMH6552 (or a similar part like LMH5401) as a fully differential transimpedance amplifier, to convert the differential current output (+/-20mA full scale range) from a high speed DAC to a voltage output line driver, to drive a 100 Ohm differential pair over some distance, let's say 10 inches?
The 100 Ohm differential pair would be a combination of matched PCB traces and twinax cable for the actual board to board connection.
The main reason for this (as opposed to a single ended signal transmission over coax) is that the DAC is located on a physically separate driver PCB, so not near the load point where the signal is needed. Using a differential signal transmission all the way to the load board should help with noise immunity and ground noise rejection.
In the simplest case, the load would be just a 50 Ohm termination with low capacitive load (less than 5pF) and it could be checked with a high quality active oscilloscope probe:

In more detail, the signal at the load would probably be converted from differential to single ended for high CMRR with another amplifier like this:

Does this look like a reasonable setup? Am I making some incorrect assumptions here?