This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA186-Q1: Application question

Part Number: INA186-Q1
Other Parts Discussed in Thread: INA186

Tool/software:

Hi expert,

My customer (CosMX) wants to use INA186-Q1 as low-side current sensing in Auto 48V BMS project. Is there any design point we need to take care in this application? Thanks.

Best Regards,

Ryker

  • Ryker,

    Thanks for the question and using the E2E forum.

    Due to the U.S. holiday we are not in the office. Someone will reply when we return on Tuesday, 9/2.

  • Hi Ryker,

    First of, the INA186 has a common mode range of -0.2V to 40V, it will not work if the bus voltage is 48V. If Vcm is within range, then the only other design note would be the input filtering, it is recommended to avoid input filtering is possible, if customer will need input filtering, ensure the R <1k and C is between 0.1 to 1uF.

    Best,
    Mallika Senthil