Part Number: THS3095
Other Parts Discussed in Thread: LMH6702, LMH6609
Tool/software:
The THS3095 is advertised as a low noise amplifier with 1.1nV/sqHz voltage and 14pA/sqHz current noise. The problem is that the datasheet recommends using a feedback resistor on the scale of 1Kohm. With these values the total noise of the circuit is much higher. For example, a G=-1 amplifier will have output noise of 15nV/sqHz due to the effects of the current noise. If I understand correctly, in order to achieve significant improvement in the output noise, a much smaller feedback resistor has to be used, something in the order of 100ohm. The datasheet does mention that smaller than 1Kohm resistors are possible, but warns from possible stability issues. Yet, there is no diagram that shows how exactly the stability is affected by a smaller feedback resistor.
Is there something I'm missing in my analysis?
Can you provide the missing information?
If 15nV/sqHz is unavoidable, is there a different amplifier that you would recommend to achieve better overall noise characteristics?
Thank you,