Part Number: THS3470REBEVM
Other Parts Discussed in Thread: THS3470
Tool/software:
Hi Support Team,
The documentation of THS3470 describes a power down mode controlled by P0 and P1 pin (No. 30 and 31). If both pins are connected to ground the power down mode is entered. The evaluation board can connect both pins to ground by switch s3.
I monitor the output signal of the THS3470 with an oscilloscope. If I switch to power down mode, the signal form changes but the signal is still on the output. I would expect that the signal is turned off in power down mode. Will this behavior change in the next IC revision? I have Rev.B.
The customer of our planed product may overload the output of THS3470. E.g. by connect a long cable or a wrong load. Will the HTS3470 be protected against overload at +-30V supply voltage when OVTEMP_FLAG (1/2) is connected to P0/P1 power control?
Thank You
Guenter