Part Number: INA187
Other Parts Discussed in Thread: INA293,
Tool/software:
Hello,
I have an existing design that is currently using an INA293A1 as a low side current sense amplifier to increase the negative common mode range for a UCC29002-1 based load sharing circuit. That circuit is showing some unexpected behavior under light loads and one of the ideas is that the negative overload recovery time of the INA293 might play a role as some of the supplies might be backdriven under light load due to power supply tolerances. See the link below for more details.
I found that the INA187 does not include this section about overload recovery in its datasheet. So if I use the INA187 as a unidirectional amplifier by tying the ref pin to the gnd pin, will it operate without this overload recovery time?
Also for the INA293A1 roughly how long would the recovery time be? I expect the most negative Vsense the INA293A1 would see would be -10mV, probably less.
RE: UCC29002: Improving current settling time and expected current waveform behavior
Thanks