Part Number: TLV8812
Tool/software:
Dear Team,
My customer is considering to use the TLV8812DGKR as non-inverting amplifier as below.

What is the lowest input voltage that an operational amplifier can output in?
In order to amplify an input voltage of about 10 mV, they want to understand the characteristics of the minimum input voltage.
If input voltage +IN is higher than VOS, is it OK?
When the TLV8812 is used in a non-inverting amplifier as shown above, is it correct to recognize that the op amp's open-loop gain is stable if +IN is greater than 0V?
Or, although the lower limit of the output voltage is described on the data sheet, is it necessary to have +in enough to output this voltage?

Best Regards,
Koshi Ninomiya