Part Number: INA169
Tool/software:
Detection current range: 0A~60A
1. Confirm RS. Is the resistance value appropriate?
2. Is the selected RL resistor value appropriate?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA169
Tool/software:
Detection current range: 0A~60A
1. Confirm RS. Is the resistance value appropriate?
2. Is the selected RL resistor value appropriate?
Thanks!
David,
I am assuming that the 0m50 resistor here for RS is 0.5mΩ, or 500uΩ. With your defined system, your maximum differential occurs at 60 amps, where V_sense would be
V_sense = 60A * 0.5mohm = 30mV
and you want that value to correspond to your highest voltage output for maximization of FSR, so ideally,
Vout = 3.3 V when V_sense = 30 mV. To achieve this, we need to select a gain for the design to achieve this, so
3.3V/.030V = 110. So a 110kΩ resistor for RL would cast the sense voltage across the entirety of the output. You can still use 22kΩ, but this would only use a portion of the output range, and also the offset voltage will be larger in proportion to the total signal.
Hope this helps. Let me know if you need anything else.
Carolus