This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA857: OPA857 Spice Model

Part Number: OPA857
Other Parts Discussed in Thread: OPA858, TINA-TI

Tool/software:

I am using the OPA857 in LTSpice and I am getting an error about floating nodes within the device:

ERROR: Node U2:I0:I5:I19:1:102 is floating and connected to current source G:U2:I0:I5:I19:1:RA
ERROR: Node U2:I0:I5:I19:1:302 is floating and connected to current source G:U2:I0:I5:I19:1:RC

u2:i0:i5:v0: Missing value, assumed 0V @ DC
u2:i0:i5:v1: Missing value, assumed 0V @ DC
Per .tran options, skipping operating point for transient analysis.
Ignoring empty pin current: Ix(u2:ctrl)

Is there an issue with the Spice model such as missing model definitions?