Part Number: OPA380
Other Parts Discussed in Thread: OPA859
Tool/software:
Hi Sir,
may we know two quesiton, and learn from you,
1. According to the reference circuit on page 11 of the datasheet, with VBIAS set to 250 mV, the output signal swing is only about 200 mV (with an input optical signal strength of -21 dBm). However, the datasheet specifies that Vout can go up to 4.4 V.
2. Using the -3 dB bandwidth calculation formula on page 11 of the datasheet, with RF = 10 kΩ, the calculated bandwidth is about 29 MHz, but in practice the circuit fails at around 4 MHz.
3. With an input optical signal of 2 MHz, 50% duty cycle, and strength from -15 dBm to -27 dBm, after amplification by the OPA380, the output only works properly at around -18 dBm to -20 dBm, producing a square wave with an amplitude of about 200 mV.
we question as below:
1. Is the OPA380 suitable for this design requirement? If not, could you suggest an appropriate TIA solution?
2. How can I ensure stable reception of optical signal strengths in the range of -15 dBm to -27 dBm?