Part Number: INA240
Tool/software:
Hello support team all.
I am attempting to measure bidirectional coil current in a circuit using an INA240A1 to control the coil current in an H-bridge circuit.
The applied voltage is 48V. The MOSFET Ron value is 20mΩ, and the maximum current is 6.25A. (See the diagram below.)
I would like to predict the output voltage of the INA240A1.

I understand that the output voltage error for the INA240A1 is calculated according to the formula in the table in 8.4.4.1 Error Sources in the datasheet.
The calculated error results are shown in the attached Excel spreadsheet.
Could you please check that these results are correct?
If the results are correct, I can assume that a large offset occurs when the common-mode voltage is low (off period), causing waveform distortion.
Is my understanding correct?
Best regards,
DH