This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS3217: usage where gain << 1 V/V

Part Number: THS3217

Tool/software:

I want to amplify a sine wave in the range of 10~800 MHz. I hope for a gain of 10 dB. Is it possible to use RF = 150Ω and RG = 240Ω? Please tell me the problems with usage where gain << 1 V/V.

  • Hi,

    I would not recommend operating the power amplifier stage at a gain lower than 1.5V/V as it will likely result in an unstable amplifier. For higher Vpp voltages it is recommended to keep the gain at 2.5V/V or above. You could consider an attenuation network using resistors at the output as an option. 

    Best Regards,

    Ignacio