Tool/software:
Hi,
Is there any way to make 2300v/v gain with INA630?
Is cascade only way for it?
Thanks.
Hey David,
What is your target application? The INA630 maximum gain is 1000, so to achieve a gain of 2300V/V, you will need to add an amplifier after the INA630 to amplify the signal further. However, there are other limiting factors like output noise that may make this not a great solution. Could you please provide more information about your application?
Best,
Gerasimos