This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903: lm2903 power up time

Part Number: LM2903
Other Parts Discussed in Thread: LM339, TLV1822

Tool/software:

what is the "power up time" of the lm2903?  i.e. the time between when Vcc exceeds a certain threshold (device on), and the outputs are correct based on the inputs?

thanks,

Stu DeJonge

Principal Engineer

  • Hello Stuart,

    The LM2903 is a simple device, and can start up within 100's of nS depending on the ramp of the supply voltage. This is a bipolar device with no POR and a simple bias generator.

    The supply voltage needs to get above 2V before it fully wakes up, then response would be similar to the lowest propagation delay.

    It should be up-and-ready after about 1-2us. Note that start-up time or minimum voltage is NOT a guaranteed parameter.

    But this is not simple as there are other forces at work.

    Please see section 10 of the LM339 family application note. This discusses power-up behavior:

    Application Design Guidelines for LM339, LM393, TL331 Family Comparators

    If specific start-up behavior is required, the TLV182x/3x/5x family has POR that ensures the output is in a specific state for a specific period after crossing minimum supply voltage.

    For example, the TLV1822 will keep the output high-Z for 200us after the supply voltage crosses 2.4V, then the output will reflect the inputs.