This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780EVM-002: How can i change the output power from 45w to 65w?

Part Number: UCC28780EVM-002


Tool/software:

Hi,

I’m testing the UCC28780EVM-002 and have two questions:

1. The EVM is rated for 45 W output. Is it possible to modify the external circuitry to achieve around 65 W output power?

2. Is it possible to measure the magnetizing inductor current waveform? If so, how can it be measured?

Thanks for your help!