Part Number: INA129
Other Parts Discussed in Thread: PGA848
Tool/software:
Hi everyone,
I'm working on a design where I need to measure the voltage drop across a current-sense resistor.
The sensor output is a differential signal with a typical range up to 0-2V, but in certain conditions (cutoff state), the differential voltage can go as high as 5V.
The instrumentation amplifier (INA129) is powered by a dual ±5V supply.
To support two measurement ranges, I’m planning to use two INA129 amplifiers:
-
One configured with gain = 1
-
The other with gain = 50
The idea is to connect both amplifiers to the same resistor (i.e., parallel inputs), and then select between their outputs downstream ( Different ADC channel).
However, I'm concerned that connecting both INA129 inputs in parallel might cause interference or loading effects between the two amplifiers, especially given their different gain configurations.
Would one amplifier load or otherwise affect the other due to the parallel input configuration?
Is there a better way to implement this dual-range measurement approach?
Any advice or experience with similar designs would be appreciated!
Thanks in advance!