AMC3302: ngspice error: expected (possibly empty) sequence of Spice lines followed by an .ends line

Part Number: AMC3302

Tool/software:

Hello,

I am using Kicad 9.0.1; see the the following info about it:

Application: x64 on x64
Version: 9.0.1, release build
Libraries:
    wxWidgets 3.2.6
    FreeType 2.13.3
    HarfBuzz 10.2.0
    FontConfig 2.15.0
    libcurl/8.11.1-DEV Schannel zlib/1.3.1
Platform: Windows 10 (build 19045), 64-bit edition, 64 bit, Little endian, wxMSW
OpenGL: NVIDIA Corporation, Quadro P2000/PCIe/SSE2, 4.6.0 NVIDIA 537.70
Build Info:
    Date: Mar 30 2025 01:11:30
    wxWidgets: 3.2.6 (wchar_t,wx containers)
    Boost: 1.86.0
    OCC: 7.8.1
    Curl: 8.11.1-DEV
    ngspice: 44
    Compiler: Visual C++ 1942 without C++ ABI
    KICAD_IPC_API=ON
Locale: 
    Lang: en_GB
    Enc: UTF-8
    Num: 1,234.5
    Encoded кΩ丈: D0BACEA9E4B888 (sys), D0BACEA9E4B888 (utf8)

After downloading from your site the PSPICE model for AMC3302 (sbam475.zip), when trying to simulate a schematic including this circuit I receive the following error:
AMC3302.lib:655:1: expected (possibly empty) sequence of Spice lines followed by an .ends line

What can be done?

Thank you in advance.