This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2994: OPA2994 Slew Rate in Datasheet not achieved

Part Number: OPA2994


Tool/software:

I am using the OPA2994IDR and require a slew rate of at least 30V/µs. I am using the OP as an inverting amplifier with a factor of 1.5. Unfortunately, I am measuring a rise time of 20V/µs at the output.

I have seen that the data sheet was changed from 18V/µs to 35V/µs in 2024. Could it be that I have received an “old” component?
Under what specific conditions is the slew rate of 35V/µs specified in the data sheet achieved?