Tool/software:
Hello, we are hoping to use the BUF802 internal clamps to clamp at +/-1V away from our 2.5V output. I tested this by setting the clamps with diodes (just like the dev kit) I used 1.8V for CLL and 3.6V for CLH, our rails are 3.5V and 8.5V so that the mid-rail sit's at 2.5V (our output).
The clamping seems to work fine but there is a major issue with bandwidth. With the clamps installed in this configuration the bandwidth is reduced dramatically. Almost as if the diode capacitance makes it to the output. The image below is a 200Mhz sweep at 200mVpp, the bandwidth drops very quickly.

When I remove the diodes and tie CLL to GND and CLH to 8.5V the bandwidth is fine (needs a bit of tuning but otherwise it's good).
Can you help with a setup that uses the internal clamps set to 1.5V and 3.5V with and output at 2.5V? Is this even possible with the internal design of the chip?
Thanks