This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP8602MAEVAL: LMP8602MAEVAL

Part Number: LMP8602MAEVAL
Other Parts Discussed in Thread: INA200

Tool/software:

Hello TI Team,

I purchased the LMP8602MAEVAL board for current monitoring in a PXI analog card.

My setup includes a 20 mΩ shunt resistor, with 15 V applied from a power supply. The load draws 1 A, resulting in a 20 mV voltage drop across the shunt.

I want to amplify this small voltage using the EVM to make it readable by my PXI ADC.

I also have an INA200 EVM available.

Could you please confirm if any modifications are needed to the EVM circuit to support this setup?
Also, which EVM would be more suitable for accurate current monitoring in this application?

Thank you!
— Shivaraj R