Other Parts Discussed in Thread: INA190, INA186
Tool/software:
Hi team,
I'm building a motor driver board where I used a INA138 to measure the supply current, because the board would consume nearly 320A at peak, so I've used 2 0.25mR resistor in parallel can connects it in a kelvin sensing fashion.


but the output is almost unuseable. Per the calculation it should have readings for around 1A, but it only starts producing output after around 5A. I almost thought the chip is broken.
and it has lots of noises too. Not sure if it came from the power supply and it just amplifed it as well. BLDC motor is indeed very noisy.

should I max out the gain RL resistor or pick a higher resistance current sense resistor?