Other Parts Discussed in Thread: OPA657, TINA-TI
Dear all,
I am trying to use OPA657 as a transimpedance amplifier but recently I met problem.
I current signal from APD is about 0.2uA (during my experiment, the current signal has very low frequency, almost DC). I set up the circuit according to the figure on the cover of OPA657 user manual, but I found the output signal on the pin6 is fixed on 0.9 V and without change even when I change the input light intensity of the APD.

the power +vs I used is 5v. Please help me on this problem, thank you.
Another phenomenon, the above phenomenon happened when I connect the Ground of Puwer supply to the Ground of amplifier (Pin 3 and Pin4). When I disconnect the Pin3&4 with power supply ground, the signal obversed from osloscope (1M impedance) can change with the intensity of inlut light. However in the later case, it seems that the amplifier does not work.


T