INA226-Q1: Spec Inquiry

Part Number: INA226-Q1
Other Parts Discussed in Thread: INA226

Hi TI Expert,

Few questions about the INA226-Q1 hope you can help to clarify:

  1. May I know how to judge whether this current sensor can support uni-direction or bi-direction if datasheet didn't mention about it?  If the VIN+ - VIN- can accept both positive/negative voltage, does that means it can support bi-directional?

image.png

 

2. May I know how to judge the Bandwidth limitation on IN+/IN- signal? Should I just use the below graph and find the related frequency range before reach -3dB gain? So for INA226-Q1, I think it will be around 400kHz, is that correct?

image.png

 

Thank you.

  • Hello Evan,

    Here are my responses to your questions:

    1. Correct, the INA226 is bi-directional.

    2. The bandwidth depends on your chosen conversion time, averaging settings, and the number of channels converting. For example, if you are converting for only the shunt voltage at 140µs, then the sample rate would be 1/140µ ≈ 7.143kHz. If you are converting for both shunt and bus voltage, with 140µs conversion on each, then your sample rate would be 1/(140µ+140µ) ≈ 3.571kHz. The plot in Figure 5-1 is for a single channel conversion of 1.1ms, which would be a sample rate of 1/(1.1m) ≈ 909Hz. From the plot, you can see that the -3dB point is approximately half of the sample rate. This will scale with your conversion settings. 

    Regards,

    Mitch

  • Hi Mitch,

    Sorry for the late response.

    So based on the info in Figure 5-1, we can just use half of the sampling rate as the frequency response rate?

     

  • Yes, that would be a good approximation of the -3dB point.