This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA226: show the power use

Part Number: INA226
Other Parts Discussed in Thread: SYSCONFIG

Hi

I want to implement this with an INA226. I plan to use it in a set-top box and show the set-top’s power use on the TV.
Can I measure voltage and current with the INA226 and send those values to the MCU?
The power shown is only the set-top’s consumption — not accounting for the adapter’s efficiency.

-Set-top SPEC-

set power : DC 5V / Max 2.5A

Thanks