Hello,
This is Moon.
I’m seeing abnormal output behavior on the TLV3802. In the attached screenshot, the orange trace is the comparator input and the green trace is the comparator output. With the threshold set to 2.1 V, I expect an output pulse width of about 7–8 ns, but the actual waveform does not match this.
The input to the comparator has a 2 V DC offset, and the supply rails are 0 V and +5 V, so I believe the common-mode range is within spec. However, the measured output shows a second LVDS transition with a width greater than 100 ns—that is, the output toggles twice (two rise–fall events).

Could you please advise on the likely cause of this behavior and recommended next steps?
Best regards,
Moon