Other Parts Discussed in Thread: OPA453, LM5113
Hi,
I'm looking to drive GaN SW that has controls . On each control I need to have 0V or -40V (prefer -60V).
I need op amp that will act like comparator when I put "0" the comparator/opamp output will be 0V
When the input is +3.3V the comparator/opamp output will be -40V .
I need to drive ~5mA at the peak and continues ~1mA.
Does the OPA453 can fit this requesets?
Thanks,
Ziv