Other Parts Discussed in Thread: INA193, INA168, INA271, INA282
Hi ,
I plan to measure a current through a sensor resistor.
Specs are following :
• Common mode : 0 to 51V
• Current : 0 to 5A
• Max drop voltage : 100mV
• Settling time : 5µs
According to specifications, it seems that the INA193 suits well to this application
The simulation given by INA193 TI PSpice project available on TI website gives weird results :
Schematic:
Results:
So it appears that for a 50mV voltage drop on RSENSE, INA193 output is about 5mV instead of 1V.
This result doesn’t match with theory.
Moreover, results go back to normal if common mode voltage is decreased from 51V to 30V.
Have you any feedback of relative to the INA193 PSpice Model, or rather have I done something wrong?
Thank you for your answer or insight to this problem.
Regards,
Jean-Baptiste OSMONT