Hi,
The XTR200 is specified for a supply voltage from 8 V (min) to 60 V (max), p.4. Will it still work with a 5 V power supply?
thank you for your feedback
Marcel
Hi Marcel,
The XTR200 has an output disable mode and will automatically disable the output when the power supply is below 7.4V. The device will not work as intended at a 5V power supply and will need to be set to the minimum supply voltage of 8V in order to operate.

Regards,
Ashley
Hello Ashley,
Thank you for your feedback, I missed that data point.
Best Regards,
Marcel